This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AM3354 's (Sitara Processor) CLKOUT2 (Clock out) as Master clock input for TLV320AIC3106?

Other Parts Discussed in Thread: AM3354

Hi ,

AM3354 has two clock outputs (CLKOUT1 & CLKOUT2) .

I'm using 24MHz crystal as clock input to the processor. Can I not use one of these clocks for Audio Codec Master clock as well as HDMI transmitter (Audio section) master clock?

If yes, then why in evaluation board external oscillator is used for Audio Codec MCLK?

http://www.ti.com/tool/tmdxevm3358

Thanks in advance.

Regards,

Sarusha