Other Parts Discussed in Thread: OMAP-L138
Hi I am using OMAP-L138 and dvsdk-version 2.6.37.
I tried loading the images in ramdisk, default ramdisk size given in kernal configuration is 32768KB. I am able to load the image.
Filesystem 1K-blocks Used Available Use% Mounted on
/dev/root 31727 30024 65 100% /
none 8 12 18014398509481980 150% /dev
tmpfs 16384 24 16360 0% /var/volatile
tmpfs 62764 0 62764 0% /dev/shm
tmpfs 16384 0 16384 0% /media/ram
But when I changed the default ramdisk size in kernel configuration: Device drivers -> Block devices.
Still the partition size is same as given above.
Can anyone pz tell me how to change the size for /dev/root.
Thanks in advance.