Hello
I was reading RTM and looking for information about nRESETIN_OUT duration. As stated in manual, nRESETIN_OUT will be kept low during PRM_RSTTIME.RSTTIME1 cycles of SYS_CLK which default value is 6h. However, the expression SYS_CLK is not used in text or diagram inside section 8.1.6 (clock generation and management).
Could clarify to which clock line SYS_CLK refers to ?
Moreover, if I want to change the nRESETIN_OUT should I set a new value for PRM_RSTTIME.RSTTIME1 and perform a warm reset ? Is this the proper approach ?
RTM Fix: please, at page 666 fix the reference for RSTTIME1. It is used PRM_DEVICE_RSTTIME1 instead PRM_RSTTIME..RSTTIME1 (fourth line).
Thanks