This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

EMIF target impedance

Support,

Can you please address this question from my customer...

"Question about PCB stackup spec in regards to the EMIF.  Table 8-68 in the datasheet specs a target impedance min of 50ohms and max of 75ohms.   It also specs an impedance control of Z+/-5 ohms.  Does this mean I can target a 50ohm line with 10% tolerance and satisfy both NO. 13 and 14 in the table?" 

Thanks,

Tim