TheConcerto PHY_Example software appears to be using DSP/BIOS rather than SYS/BIOS. What is the proper procedure for adding a task and associated conditions? I have tried following the procedure in the CCS4 help for DSP/BIOS 5.41.11.38, but there is no "Target Content" window.
For the F28M35H52C1, I select C2000, device variant F28M35H52C1, DSP/BIOS v5.xx Examples but - no F28M35x28x examples show. If I select control28069, hello example, I get the error: Internal Error, "java.lang.NullPointerException: . If I select SYS/BIOS Examples, then 28x Examples, then Task Example, I get the same error. IsHow do I add a task to the PHY_Example? my CCS corrupted? What should happen here? Are there anny F28M35xx examples?
Thanks,
Pat