Other Parts Discussed in Thread: SYSBIOS
Dear all:
on page 7th of DM814x_EZ_Software_Developers_Guide.gdf , i know the codec engine examples can not be run out with graphics,so i execute "/etc/init.d/load-hd-firmware.sh stop " , the codec engine application can run on the dm8148 evm board.If i want to add hmi for codec engine application, how do i for it?here ,i have some questions as follow:
Q1, http://processors.wiki.ti.com/index.php/EZSDK_Memory_Map shows the EZSDK's memory allocation
DSP_CODE SIZE = 0M, if i run codec on the c674 dsp core ,how to specify the DSP_CODE memory segment?
Q2, DM814x_EZ_Software_Developers_Guide.gdf tell us that codec engine examples can not be run out with graphics,what about codec engine examples and viddeo m3 can run at the same time?
Q3,http://processors.wiki.ti.com/index.php/EZSDK_Memory_Map , i change memory map for 512Mb dm8148 board. my dsp configure files are below:
config.bld:
/*
* ======== config.bld ========
* This script is run prior to all build scripts. It initializes the
* rootDir configuration parameter of all supported targets.
*
* There are more details about config.bld here:
* http://rtsc.eclipse.org/docs-tip/Glossary#config.bld
*/
var Build = xdc.useModule('xdc.bld.BuildEnvironment');
var Pkg = xdc.useModule('xdc.bld.PackageContents');
/* initialize local vars with those set in xdcpaths.mak (via XDCARGS) */
for (x = 0; x < arguments.length; x++) {
if (arguments[x].match(/^CODEGEN_INSTALL_DIR=/)) {
cgRootDir = arguments[x].split("=")[1];
}
}
var mem_ext = [
["DDR3_HOST", {
comment: "DDR3 Memory reserved for use by the A8",
name: "DDR3_HOST",
base: 0x80000000,
len: 0x0B000000,
}
],
["DDR3_data", {
comment: "DDR3 Memory reserved for use by the C674",
name: "DDR3_data",
base: 0x99500000,
len: 0x00800000,
}
],
["DDR3", {
comment: "DDR3 Memory reserved for use by the C674",
name: "DDR3",
base: 0x99D00000,
len: 0x00400000,
}
],
["DDRALGHEAP", {
comment: "DDRALGHEAP: off-chip memory for dynamic allocation",
name: "DDRALGHEAP",
base: 0x98000000,
len: 0x01400000,
}
],
["DDR3_SR1", {
comment: "DDR3 Memory reserved for use by SharedRegion 1",
name: "DDR3_SR1",
base: 0x9A100000,
len: 0x00100000,
}
],
["DDR3_SR0", {
comment: "DDR3 Memory reserved for use by SharedRegion 0",
name: "DDR3_SR0",
base: 0x99400000,
len: 0x00100000 /* 1 MB */
}
],
];
/* platform instances used by this package */
Build.platformTable["ti.platforms.evmDM8148"] = {
externalMemoryMap: mem_ext,
l1DMode:"32k",
l1PMode:"32k",
l2Mode:"128k",
codeMemory: "DDR3",
dataMemory: "DDR3_data",
stackMemory: "DDR3"
};
/* should test here that cgRootDir is set! */
var C674 = xdc.useModule('ti.targets.elf.C674');
C674.rootDir = cgRootDir;
C674.platforms = [
"ti.platforms.evmDM8148"
];
$trace("Adding ti.targets.elf.C674 to Build.targets", 1, ['genserver']);
Build.targets.$add(C674);
/* We remove a few profiles, just to cut down on build time */
delete C674.profiles["coverage"];
delete C674.profiles["profile"];
delete C674.profiles["whole_program"];
delete C674.profiles["whole_program_debug"];
/* Create a .zip file for redistribution. Remove this line if you prefer .tar */
Pkg.attrs.archiver = 'zip';
server.cfg:
/*
* ======== server.cfg ========
*
*/
/* scratch groups */
var MAXGROUPS = 20;
var GROUP_2 = 2;
$trace("platformName = '" + Program.platformName + "'", 1, ['genserver']);
function createHeapMem(size, sectionName, heapName) {
var HeapMem = xdc.useModule('ti.sysbios.heaps.HeapMem');
var heapMemParams = new HeapMem.Params();
heapMemParams.size = size;
heapMemParams.sectionName = sectionName;
Program.sectMap[sectionName] = heapName;
return HeapMem.create(heapMemParams);
}
/* heap config */
var internalMemoryName = 'IRAM';
var internalHeapSize = 0xc000; // 48 kB
var externalMemoryName = 'DDR3';
var externalHeapSize = 0x20000; // 128 kB
/* Configure internal and external heaps */
Program.global.EXT_HEAP =
createHeapMem(externalHeapSize, ".EXT_HEAP", externalMemoryName);
Program.global.INT_HEAP =
createHeapMem(internalHeapSize, ".INT_HEAP", internalMemoryName);
var DDRALGMemoryName = "DDRALGHEAP";
var DDRALGHeapSize = Program.platform.externalMemoryMap[DDRALGMemoryName].len;
Program.global.EXTALG_HEAP = createHeapMem(DDRALGHeapSize, ".EXTALG_HEAP", DDRALGMemoryName);
/* Place code */
Program.sectMap[".text"] = externalMemoryName;
/* Set the default heap to the external heap */
var Memory = xdc.useModule('xdc.runtime.Memory');
Memory.defaultHeapInstance = Program.global.EXT_HEAP;
/* end heap config */
/* Setup xdcruntime proxys */
xdc.useModule('ti.sysbios.xdcruntime.Settings');
/*
* Configure CE's OSAL. This codec server only builds for the BIOS-side of
* a heterogeneous system, so use the "DSPLINK_BIOS" configuration.
*/
var osalGlobal = xdc.useModule('ti.sdo.ce.osal.Global');
osalGlobal.runtimeEnv = osalGlobal.DSPLINK_BIOS;
var Timer = xdc.useModule('ti.sysbios.timers.dmtimer.Timer');
Timer.intFreq.hi = 0;
Timer.intFreq.lo = 20000000;
/* IPC-related config */
xdc.useModule('ti.sdo.ce.ipc.dsplink.dsp.Settings');
var MultiProc = xdc.useModule('ti.sdo.utils.MultiProc');
var settings = xdc.useModule('ti.sdo.ipc.family.Settings');
var procNames = settings.getDeviceProcNames();
MultiProc.setConfig("DSP", procNames);
var SharedRegion_map = {};
SharedRegion_map["SysLink: HOST<--->DSP"] = 0;
SharedRegion_map["Ipc"] = 1;
var SharedRegion = xdc.useModule('ti.sdo.ipc.SharedRegion');
var syslinkSharedMem = Program.cpu.memoryMap["DDR3_SR0"];
var ipcSharedMem = Program.cpu.memoryMap["DDR3_SR1"];
var entry = new SharedRegion.Entry();
entry.base = syslinkSharedMem.base;
entry.len = syslinkSharedMem.len;
entry.ownerProcId = MultiProc.getIdMeta("HOST");
entry.isValid = true;
entry.name = "SYSLINK";
SharedRegion.setEntryMeta(
SharedRegion_map["SysLink: HOST<--->DSP"], /* index */
entry
);
var entry2 = new SharedRegion.Entry();
entry2.base = ipcSharedMem.base;
entry2.len = ipcSharedMem.len;
entry2.ownerProcId = MultiProc.getIdMeta("HOST");
entry2.isValid = true;
entry2.createHeap = true;
entry2.cacheEnable = true;
entry2.name = "SR1";
SharedRegion.setEntryMeta(
SharedRegion_map["Ipc"], /* index */
entry2
);
/*
* ======== Server Configuration ========
*/
var Server = xdc.useModule('ti.sdo.ce.Server');
/* The server's stackSize. More than we need... but safe. */
Server.threadAttrs.stackSize = 16384;
/* The servers execution priority */
Server.threadAttrs.priority = Server.MINPRI;
xdc.loadCapsule('server_log.cfg');
/*
* The optional stack pad to add to non-configured stacks. This is well
* beyond most codec needs, but follows the approach of "start big and
* safe, then optimize when things are working."
*/
Server.stackSizePad = 9000;
/*
* "Use" the various codec modules; i.e., implementation of codecs.
* All these "xdc.useModule" commands provide a handle to the codecs,
* which we'll use to initialize config params and add the codecs to
* the Server.algs array.
*/
var DARKLIGHT = xdc.useModule('adas.darklight.DARKLIGHT');
DARKLIGHT.serverFxns = "UNIVERSAL_SKEL";
DARKLIGHT.stubFxns = "UNIVERSAL_STUBS";
DARKLIGHT.manageInBufsCache = [true, true, true, true, true, true, true, true, true, true, true, true, true, true, true, true];
DARKLIGHT.manageInOutBufsCache = [true, true, true, true, true, true, true, true, true, true, true, true, true, true, true, true];
DARKLIGHT.manageOutBufsCache = [true, true, true, true, true, true, true, true, true, true, true, true, true, true, true, true];
/*
* The array of algorithms this server can serve up. This array also
* configures details about the threads which will be created to run the
* algorithms (e.g. stack sizes, priorities, etc.).
*/
Server.algs = [
{name: "darklight", mod: DARKLIGHT , threadAttrs: {
stackMemId: 0, priority: Server.MINPRI + 1},
groupId : 2,
},
];
/* to link in debug/trace FC libs, uncomment one of these */
// xdc.useModule('ti.sdo.fc.global.Settings').profile = "debug");
// xdc.useModule('ti.sdo.fc.global.Settings').profile = "debug_trace");
// xdc.useModule('ti.sdo.fc.global.Settings').profile = "trace");
/*
* ======== DSKT2 (XDAIS Alg. memory allocation) configuration ========
*
* DSKT2 is the memory manager for all algorithms running in the system,
* granting them persistent and temporary ("scratch") internal and external
* memory. We configure it here to define its memory allocation policy.
*
* DSKT2 settings are critical for algorithm performance.
*
* First we assign various types of algorithm internal memory (DARAM0..2,
* SARAM0..2,IPROG, which are all the same on a C64+ DSP) to "L1DHEAP"
* defined in the .tcf file as an internal memory heap. (For instance, if
* an algorithm asks for 5K of DARAM1 memory, DSKT2 will allocate 5K from
* L1DHEAP, if available, and give it to the algorithm; if the 5K is not
* available in the L1DHEAP, that algorithm's creation will fail.)
*
* The remaining segments we point to the "DDRALGHEAP" external memory segment
* (also defined in the.tcf) except for DSKT2_HEAP which stores DSKT2's
* internal dynamically allocated objects, which must be preserved even if
* no codec instances are running, so we place them in "DDR2" memory segment
* with the rest of system code and static data.
*/
var DSKT2 = xdc.useModule('ti.sdo.fc.dskt2.DSKT2');
DSKT2.DARAM0 = "INT_HEAP";
DSKT2.DARAM1 = "INT_HEAP";
DSKT2.DARAM2 = "INT_HEAP";
DSKT2.SARAM0 = "INT_HEAP";
DSKT2.SARAM1 = "INT_HEAP";
DSKT2.SARAM2 = "INT_HEAP";
DSKT2.ESDATA = "EXTALG_HEAP";
DSKT2.IPROG = "INT_HEAP";
DSKT2.EPROG = "EXTALG_HEAP"
DSKT2.DSKT2_HEAP = "EXT_HEAP";
/*
* Next we define how to fulfill algorithms' requests for fast ("scratch")
* internal memory allocation; "scratch" is an area an algorithm writes to
* while it processes a frame of data and is discarded afterwards.
*
* First we turn off the switch that allows the DSKT2 algorithm memory manager
* to give to an algorithm external memory for scratch if the system has run
* out of internal memory. In that case, if an algorithm fails to get its
* requested scratch memory, it will fail at creation rather than proceed to
* run at poor performance. (If your algorithms fail to create, you may try
* changing this value to "true" just to get it running and optimize other
* scratch settings later.)
*
* Setting "algorithm scratch sizes", is a scheme we use to minimize internal
* memory resources for algorithms' scratch memory allocation. Algorithms that
* belong to the same "scratch group ID" -- field "groupId" in the algorithm's
* Server.algs entry above, reflecting the priority of the task running the
* algorithm -- don't run at the same time and thus can share the same
* scratch area. When creating the first algorithm in a given "scratch group"
* (between 0 and 19), a shared scratch area for that groupId is created with
* a size equal to SARAM_SCRATCH_SIZES[<alg's groupId>] below -- unless the
* algorithm requests more than that number, in which case the size will be
* what the algorithm asks for. So SARAM_SCRATCH_SIZES[<alg's groupId>] size is
* more of a groupId size guideline -- if the algorithm needs more it will get
* it, but getting these size guidelines right is important for optimal use of
* internal memory. The reason for this is that if an algorithm comes along
* that needs more scratch memory than its groupId scratch area's size, it
* will get that memory allocated separately, without sharing.
*
* This DSKT2.SARAM_SCRATCH_SIZES[<groupId>] does not mean it is a scratch size
* that will be automatically allocated for the group <groupId> at system
* startup, but only that is a preferred minimum scratch size to use for the
* first algorithm that gets created in the <groupId> group, if any.
*
* (An example: if algorithms A and B with the same groupId = 0 require 10K and
* 20K of scratch, and if SARAM_SCRATCH_SIZES[0] is 0, if A gets created first
* DSKT2 allocates a shared scratch area for group 0 of size 10K, as A needs.
* If then B gets to be created, the 20K scratch area it gets will not be
* shared with A's -- or anyone else's; the total internal memory use will be
* 30K. By contrast, if B gets created first, a 20K shared scratch will be
* allocated, and when A comes along, it will get its 10K from the existing
* group 0's 20K area. To eliminate such surprises, we set
* SARAM_SCRATCH_SIZES[0] to 20K and always spend exactly 20K on A and B's
* shared needs -- independent of their creation order. Not only do we save 10K
* of precious internal memory, but we avoid the possibility that B can't be
* created because less than 20K was available in the DSKT2 internal heaps.)
*
* Finally, note that if the codecs correctly implement the
* ti.sdo.ce.ICodec.getDaramScratchSize() and .getSaramScratchSize() methods,
* this scratch size configuration can be autogenerated by
* configuring Server.autoGenScratchSizeArrays = true.
*/
DSKT2.ALLOW_EXTERNAL_SCRATCH = false;
//DSKT2.SARAM_SCRATCH_SIZES[GROUP_2] = 0x0000;
DSKT2.DARAM_SCRATCH_SIZES[GROUP_2] = 0x0000;
DSKT2.SARAM_SCRATCH_SIZES[GROUP_2] = 32 * 1024;
/*
* ======== DMAN3 (DMA manager) configuration ========
*/
/* First we configure how DMAN3 handles memory allocations:
*
* Essentially the configuration below should work for most codec combinations.
* If it doesn't work for yours -- meaning an algorithm fails to create due
* to insufficient internal memory -- try the alternative (commented out
* line that assigns "DDRALGHEAP" to DMAN3.heapInternal).
*
* What follows is an FYI -- an explanation for what the alternative would do:
*
* When we use an external memory segment (DDRALGHEAP) for DMAN3 internal
* segment, we force algorithms to use external memory for what they think is
* internal memory -- we do this in a memory-constrained environment
* where all internal memory is used by cache and/or algorithm scratch
* memory, pessimistically assuming that if DMAN3 uses any internal memory,
* other components (algorithms) will not get the internal memory they need.
*
* This setting would affect performance very lightly.
*
* By setting DMAN3.heapInternal = <external-heap> DMAN3 *may not* supply
* ACPY3_PROTOCOL IDMA3 channels the protocol required internal memory for
* IDMA3 channel 'env' memory. To deal with this catch-22 situation we
* configure DMAN3 with hook-functions to obtain internal-scratch memory
* from the shared scratch pool for the associated algorithm's
* scratch-group (i.e. it first tries to get the internal scratch memory
* from DSKT2 shared allocation pool, hoping there is enough extra memory
* in the shared pool, if that doesn't work it will try persistent
* allocation from DMAN3.internalHeap).
*/
var DMAN3 = xdc.useModule('ti.sdo.fc.dman3.DMAN3');
DMAN3.heapInternal = "INT_HEAP"; /* INT_HEAP is an internal segment */
DMAN3.heapExternal = "EXTALG_HEAP";
DMAN3.idma3Internal = false;
DMAN3.scratchAllocFxn = "DSKT2_allocScratch";
DMAN3.scratchFreeFxn = "DSKT2_freeScratch";
/* Next, we configure all the physical resources that DMAN3 is granted
* exclusively. These settings are optimized for the DSP on DM6446 (DaVinci).
*
* We assume PaRams 0..79 are taken by the Arm drivers, so we reserve
* all the rest, up to 127 (there are 128 PaRam sets on DM6446).
* DMAN3 takes TCC's 32 through 63 (hence the High TCC mask is 0xFFFFFFFF
* and the Low TCC mask is 0). Of the 48 PaRams we reserved, we assign
* all of them to scratch group 0; similarly, of the 32 TCCs we reserved,
* we assign all of them to scratch group 0.
*
* If we had more scratch groups with algorithms that require EDMA, we would
* split those 48 PaRams and 32 TCCs appropriately. For example, if we had
* a video encoder alg. in group 0 and video decoder alg. in group 1, and they
* both needed a number of EDMA channels, we could assing 24 PaRams and 16
* TCCs to Groups [0] and [1] each. (Assuming both algorithms needed no more
* than 24 channels to run properly.)
*/
DMAN3.qdmaPaRamBase = 0x09004000;
DMAN3.paRamBaseIndex = 80; // 1st EDMA3 PaRAM set available for DMAN3
DMAN3.numQdmaChannels = 8; // number of device's QDMA channels to use
DMAN3.qdmaChannels = [0,1,2,3,4,5,6,7]; // choice of QDMA channels
//to use
DMAN3.numPaRamEntries = 48; // number of PaRAM sets exclusively used
//by DMAN
DMAN3.numPaRamGroup[GROUP_2] = 48; //number of PaRAM sets for scratch group 0
DMAN3.numTccGroup[GROUP_2] = 32; //number of TCCs assigned to scratch group 0
DMAN3.tccAllocationMaskL = 0; // bit mask indicating which TCCs 0..31
//to use
DMAN3.tccAllocationMaskH = 0xffffffff; // assign all TCCs 32..63 for DMAN
//DMAN3.paRamBaseIndex = 80; // 1st EDMA3 PaRAM set available for DMAN3
//DMAN3.numQdmaChannels = 8; // number of device's QDMA channels to use
//DMAN3.qdmaChannels = [0,1,2,3,4,5,6,7]; // choice of QDMA channels to use
//DMAN3.numPaRamEntries = 48; // number of PaRAM sets exclusively used by DMAN
//DMAN3.numPaRamGroup[GROUP_2] = 0; // number of PaRAM sets for scratch group 2
//DMAN3.numTccGroup[GROUP_2] = 0; // number of TCCs assigned to scratch group 2
//DMAN3.tccAllocationMaskL = 0; // assign no TCCs 0..31 for DMAN3
//DMAN3.tccAllocationMaskH = 0xffffffff; // assign all TCCs 32..63 for DMAN3
/* The remaining DMAN3 configuration settings are as defined in ti.sdo.fc.DMAN3
* defaults. You may need to override them to add more QDMA channels and
* configure per-scratch-group resource sub-allocations.
*/
/*
* ======== RMAN (IRES Resource manager) configuration ========
*/
var RMAN = xdc.useModule('ti.sdo.fc.rman.RMAN');
RMAN.useDSKT2 = true;
RMAN.tableSize = 10;
/* The lock/unlock/set/getContext functions will default to DSKT2 */
how Modify Memory Map to run codec engine app with graphics?