Hi,
I'm using the C6748 EVM on the Zoom Development Kit as supplied by LogicPD. I want to use a higher clock frequency for our DSP/BIOS project (v 5.41.13.42). I'm also using the BIOSPSP drivers (v 01.30.01). In order to increase the clock frequency, I'm aware that I have to change this in the gel file, but also in the soc_C6748.h header file that was supplied with BIOSPSP and consequently recompile BIOSPSP.
I did rebuild the BIOSPSP drivers that I required, but I did this in CCS5.2, and not in CCS4 as in the supplied project, since I do not trust the import wizard. I successfully recompiled BIOSPSP and linked it to my project with the new clock frequency (450MHz) and updated the gel file as well. However, it still does not work.
Is there any other limitations from either the hardware or PSP drivers that I'm missing here? I'm not exactly sure what else I can do, please help!
Regards
Reinier