Hi,
I test the evm6678l nand write speed via NandWriteDataBytes(), and the result is about 300KB/s which is far from the chip program speed.
My questions are:
1. how to improve the program speed ?
2. the NAND device(Numonyx NAND512R3A2DZA6E) on the evm has the page size of 528 Bytes. Replacing it with a large page size NAND may help improving the program speed. Could Ti provide a alternative NAND device which has full pins compatibility ?
Regards,
dp