Hi there,
I'm currently working on a project which requires me to build a single device incorporating a DSP. It would look something like a handheld Sound Level Meter.
I require a battery power supply inbuilt on to the same device within the device enclosure. I read on the manual that there are 2 possible power connections. Ie J5 and J6.
Considering J5 is a main power supply, I guess it would not be appropriate to utilize this connection.
J6 however, requires a molex #15-24-4041, which would be connected to a laptop or PC. What kind of connection is this? ie how will it connect to the PC via which port?
ALSO, it seems the molex #15-24-4041 part is OBSOLETE. Any replacements for this?
AND, would it be possible or advisable if I use J6 to connect to a battery supply ie AA batteries?
IF not, how would we supply power to the board with batteries?
thanks! appreciate it
Jason