Hi
I got this exception while running my code via JTGA on EVM6670.Please check
regards
Soumya
[C66XX_0] A0=0x0 A1=0x1
[C66XX_0] A2=0x0 A3=0x83cf68b0
[C66XX_0] A4=0x0 A5=0x0
[C66XX_0] A6=0x8 A7=0x0
[C66XX_0] A8=0x14ff0000 A9=0x2
[C66XX_0] A10=0x83cf68b0 A11=0x0
[C66XX_0] A12=0x0 A13=0x0
[C66XX_0] A14=0x0 A15=0x0
[C66XX_0] A16=0x83c51cd4 A17=0x0
[C66XX_0] A18=0x83c51ca4 A19=0x20
[C66XX_0] A20=0x0 A21=0x0
[C66XX_0] A22=0x88a3509c A23=0x88a34e54
[C66XX_0] A24=0x88a34e54 A25=0x0
[C66XX_0] A26=0x5bf500 A27=0x63
[C66XX_0] A28=0x3d57e4 A29=0x63
[C66XX_0] A30=0x83c53e90 A31=0x83d95488
[C66XX_0] B0=0x1 B1=0x66a0010
[C66XX_0] B2=0x0 B3=0x88c9b590
[C66XX_0] B4=0x0 B5=0x0
[C66XX_0] B6=0x83cf68b0 B7=0x83cf6740
[C66XX_0] B8=0x80002928 B9=0x15000102
[C66XX_0] B10=0x83cf68a8 B11=0x0
[C66XX_0] B12=0x0 B13=0x0
[C66XX_0] B14=0x88d34ca8 B15=0x83cf6880
[C66XX_0] B16=0x88a24a6c B17=0x0
[C66XX_0] B18=0x0 B19=0x3ff00000
[C66XX_0] B20=0x0 B21=0x801182c8
[C66XX_0] B22=0xf B23=0x0
[C66XX_0] B24=0x40008000 B25=0xa
[C66XX_0] B26=0x3fd678 B27=0x88a34f88
[C66XX_0] B28=0x88824b74 B29=0x0
[C66XX_0] B30=0x1 B31=0x83c51e8c
[C66XX_0] NTSR=0x1020f
[C66XX_0] ITSR=0xf
[C66XX_0] IRP=0x88cda294
[C66XX_0] SSR=0x0
[C66XX_0] AMR=0x0
[C66XX_0] RILC=0x0
[C66XX_0] ILC=0x0
[C66XX_0] Exception at 0x0
[C66XX_0] EFR=0x2 NRP=0x0
[C66XX_0] Internal exception: IERR=0x1
[C66XX_0] Instruction fetch exception
[C66XX_0] ti.sysbios.family.c64p.Exception: line 248: E_exceptionMin: pc = 0x88cda294, sp = 0x83cf6880.
[C66XX_0] To see more exception detail, use ROV or set 'ti.sysbios.family.c64p.Exception.enablePrint = true;'
[C66XX_0] xdc.runtime.Error.raise: terminating execution