This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

mpeg2dec cannot decode the transport stream MP@ML for HD.

Hi

I have a problem related to the mpeg2. The elementary stream is MP@ML for HD, which is working wit the dvsdk_2_00_00_22 (cs2dm6467_1_00_00_10). As we need the H.264 update, I use the dvsdk_3_10_00_19 (cs2dm6467_1_00_00_10). It is not working with this stream anymore. I tried the CE_DEBUG=3 to see anything special in the DSP communication. I don't see any different. The attached file is the

Bug5342_Jul5_1.txt (dvsdk_3_10_00_19 version)

Bug5342_sw134_Jul5_1.txt (dvsdk_2_00_00_22 version)

0045.Bug5342_sw134_Jul5_1.txt

8055.Bug5342_Jul5_1.TXT

0647.test.zip

elementary stream file.

 

Best Regards,

Philip Lee