Hi, expoerts:
DM8168 is powerful in video process, but it's weak in video input. It only supports up to four 8-bit ports, I saw some chips only support BT656 10bit, can it interface to 8-bit VIP with just ignoring the two LSB bits?
Regards
Peter
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi, expoerts:
DM8168 is powerful in video process, but it's weak in video input. It only supports up to four 8-bit ports, I saw some chips only support BT656 10bit, can it interface to 8-bit VIP with just ignoring the two LSB bits?
Regards
Peter
Hi,
Yes that should work.
Regards,
Hardik Shah
Hi,
Please mark question as answered, so that other can see it resolved.
Regards,
Hardik Shah