This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DCAN demo in StarterWare on an EVM AM335x



I’m trying to test the DCAN demo on StarterWare 02_00_00_06 on a TI EVM AM335x board but I can’t get it to work. I have flashed a SD-card with the prebuilt MLO and and APP binary and this works fine when I boot in profile 0 (SW8 0000), StarterWare starts and I can click around on the touch screen watching demos and so on. I restart the EVM in profile 1 (SW8 1000), which according to the User Guide documentation shall be set in this mode to be able to run the DCAN demo applications.  When set the switch(SW8) to profile 1 the EVM doesn’t boot correctly, it get’s stuck on the splash screen. I have serial terminal window connected to the EVM, but no information is outputted, nor can I input any information. I don’t have a CAN connection to a second EVM during this.

What am I doing wrong here?

Do I need a second EVM connected over CAN for the first EVM to boot correctly? (I understand that I need this to be able to do the full demo, but first of I’m just interested in getting executing one of the applications DCANTxRx and DCANLpBk on one EVM  because I have PC with a CAN dongle)

What exactly is the difference between profile 0 and profile 1 on the EVM AM335x?