Other Parts Discussed in Thread: ADS8556, ADS8361EVM, DAC8831EVM
Hi,
I planned to plug in an ADS8556 EVM AND a DAC7741EVM TOGETHER onto a 5-6K interface board, which was to be connected to a C6713 DSK. Since both the EVMs are parallel they did NOT fit on the 5-6K TOGETHER , but sadly I found this out only after unpacking the boxes :(
Now, I have selected again two serial SPI EVMs, the ADS8361EVM and DAC8831EVM. I want to put them TOGETHER on a 5-6K interface board. I will also plug in at the same time two DAP Signal conditioning boards one unipolar and one bipolar.
I have checked, googled asked around and THINK all these four will fit TOGETHER on a 5-6K board. If I am wrong can any one PLEASE tell me so before I order again.
Any response will be HIGHLY appreciated!!!