Other Parts Discussed in Thread: OMAP-L137, OMAPL138
WE are using Omap-L137 and trying to build a SYSLink example project using the examples provided.
WE are using CCS 5 .
After attempting to run the example project in the SYSlink installation directory to be more specific the fallowing one
SYSLink_install_dir\syslink_2_10_06_28\examples\archive\ti_platforms_evmOMAPL138_elf_linux\ex02_messageq\ex02_messageq
From reading the readme file located at SYSLink_install_dir\syslink_2_10_06_28\examples\archive
Few questions had come up:
How to install SYSLink using windows 7 operating system
How to configured and built SYSLink for the device/platform being used.
How to run "make syslink" from the top-level SysLink installation before buiding the examples.
How to pre-build slaveloader application
and then Run "make samples-hlos" from the top-level
SysLink installation before executing "make install" in each of the examples.
How to do all that in windows.
Do I have to use Linux to be able to set up a SYSlink
Thank you for the help in advance
Kassem