This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Is it serious of such warnings: "warning #10247-D: creating output section ".far" without a SECTIONS"?

Hi,

I am trying to run the FFT example from DSPLIB on C66xx. The building process generates such warnings, see below please.

Do I have to take care of them?

 

Thanks.

....................

"C:/ti/dsplib_c66x_3_1_0_0/examples/fft_example.c"

'Finished building: C:/ti/dsplib_c66x_3_1_0_0/examples/fft_example.c'

' '

'Building target: FFT_Example_66_LE_COFF.out'

'Invoking: C6000 Linker'

"C:/Program Files (x86)/Texas Instruments/C6000 Code Generation Tools 7.4.0B2/bin/cl6x" -mv6600 -g --display_error_number --diag_warning=225 --mem_model:data=far --abi=eabi --debug_software_pipeline -k -z -m"FFT_Example_66_LE_COFF.map" --warn_sections -i"C:/Program Files (x86)/Texas Instruments/C6000 Code Generation Tools 7.4.0B2/lib" -i"C:/Program Files (x86)/Texas Instruments/C6000 Code Generation Tools 7.4.0B2/include" --reread_libs --rom_model -o "FFT_Example_66_LE_COFF.out"  "./gen_twiddle_fft32x32.obj" "./gen_twiddle_fft16x32.obj" "./gen_twiddle_fft16x16.obj" "./fft_example.obj" -l"C:\ti\dsplib_c66x_3_1_0_0\lib\dsplib.ae66" -l"rts6600_elf.lib" "../C6678.cmd"

<Linking>

warning #10247-D: creating output section ".far" without a SECTIONS

   specification

warning #10247-D: creating output section ".fardata" without a SECTIONS

   specification

warning #10247-D: creating output section ".stack" without a SECTIONS

   specification

warning #10247-D: creating output section ".text" without a SECTIONS

   specification

warning #10247-D: creating output section ".cinit" without a SECTIONS

   specification

warning #10210-D: creating ".stack" section with default size of 0x400; use the

   -stack option to change the default size

'Finished building target: FFT_Example_66_LE_COFF.out'

' '

**** Build Finished ****

  • I attach the main source .c file here. It has no assembly function. Why it generates such warnings? Is it because the DSPLIB function call? I do not know what settings these dsplib func requires.

    Thanks

     

     

     

    /* ======================================================================= */
    /* fft_example.c -- FFT Example File                                       */
    /*                                                                         */
    /* Rev 0.0.1                                                               */
    /*                                                                         */
    /* Copyright (C) 2011 Texas Instruments Incorporated - http://www.ti.com/  */ 
    /*                                                                         */
    /*                                                                         */
    /*  Redistribution and use in source and binary forms, with or without     */
    /*  modification, are permitted provided that the following conditions     */
    /*  are met:                                                               */
    /*                                                                         */
    /*    Redistributions of source code must retain the above copyright       */
    /*    notice, this list of conditions and the following disclaimer.        */
    /*                                                                         */
    /*    Redistributions in binary form must reproduce the above copyright    */
    /*    notice, this list of conditions and the following disclaimer in the  */
    /*    documentation and/or other materials provided with the               */
    /*    distribution.                                                        */
    /*                                                                         */
    /*    Neither the name of Texas Instruments Incorporated nor the names of  */
    /*    its contributors may be used to endorse or promote products derived  */
    /*    from this software without specific prior written permission.        */
    /*                                                                         */
    /*  THIS SOFTWARE IS PROVIDED BY THE COPYRIGHT HOLDERS AND CONTRIBUTORS    */
    /*  "AS IS" AND ANY EXPRESS OR IMPLIED WARRANTIES, INCLUDING, BUT NOT      */
    /*  LIMITED TO, THE IMPLIED WARRANTIES OF MERCHANTABILITY AND FITNESS FOR  */
    /*  A PARTICULAR PURPOSE ARE DISCLAIMED. IN NO EVENT SHALL THE COPYRIGHT   */
    /*  OWNER OR CONTRIBUTORS BE LIABLE FOR ANY DIRECT, INDIRECT, INCIDENTAL,  */
    /*  SPECIAL, EXEMPLARY, OR CONSEQUENTIAL DAMAGES (INCLUDING, BUT NOT       */
    /*  LIMITED TO, PROCUREMENT OF SUBSTITUTE GOODS OR SERVICES; LOSS OF USE,  */
    /*  DATA, OR PROFITS; OR BUSINESS INTERRUPTION) HOWEVER CAUSED AND ON ANY  */
    /*  THEORY OF LIABILITY, WHETHER IN CONTRACT, STRICT LIABILITY, OR TORT    */
    /*  (INCLUDING NEGLIGENCE OR OTHERWISE) ARISING IN ANY WAY OUT OF THE USE  */
    /*  OF THIS SOFTWARE, EVEN IF ADVISED OF THE POSSIBILITY OF SUCH DAMAGE.   */
    /*                                                                         */
    /*        This example demonstrates the usage of the various FFT kernels   */
    /*        provided with the C6x DSPLIB. The example shows:                 */
    /*        - Twiddle factor generation for the various kernels              */
    /*        - Scaling that needs to be applied to get similar output         */
    /*          when using different kernels                                   */
    /*        - Demonstrates the usage of FFT APIs                             */
    /*                                                                         */
    /* ----------------------------------------------------------------------- */
    /*            Copyright (c) 2011 Texas Instruments, Incorporated.          */
    /*                           All Rights Reserved.                          */
    /* ======================================================================= */
    
    #include <stdint.h>
    #include <math.h>
    #include "C:/ti/dsplib_c66x_3_1_0_0/inc/dsplib.h"
    
    #include "gen_twiddle_fft16x16.h"
    #include "gen_twiddle_fft16x32.h"
    #include "gen_twiddle_fft32x32.h"
    
    /* Global definitions */
    /* Number of samples for which FFT needs to be calculated */
    #define N 256 
    /* Number of unique sine waves in input data */
    #define NUM_SIN_WAVES 4
    
    /* 
        Scale need to be applied (1/2^SCALE) to input data for 16x32 and 32x32
        FFT for their output to match 16x16. This is dure to the inherent 
        scaling present in 16x16 kernel
    */
    #define SCALE    3     
    
    
    /* Align the tables that we have to use */
    #pragma DATA_ALIGN(x_ref, 8);
    int32_t x_ref [2*N];
    
    #pragma DATA_ALIGN(x_16x16, 8);
    int16_t x_16x16 [2*N];
    #pragma DATA_ALIGN(y_16x16, 8);
    int16_t y_16x16 [2*N];
    #pragma DATA_ALIGN(w_16x16, 8);
    int16_t w_16x16 [2*N];
    
    #pragma DATA_ALIGN(x_16x32, 8);
    int32_t x_16x32 [2*N];
    #pragma DATA_ALIGN(y_16x32, 8);
    int32_t y_16x32 [2*N];
    #pragma DATA_ALIGN(w_16x32, 8);
    int16_t w_16x32 [2*N];
    
    #pragma DATA_ALIGN(x_32x32, 8);
    int32_t x_32x32 [2*N];
    #pragma DATA_ALIGN(y_32x32, 8);
    int32_t y_32x32 [2*N];
    #pragma DATA_ALIGN(w_32x32, 8);
    int32_t w_32x32 [2*N];
    
    /*  
        This function generates the input data and also updates the 
        input data arrays used by the various FFT kernels
    */
    float x_ref_float [2*N];
    void generateInput (int32_t numSinWaves) {
        int32_t i, j;
        float sinWaveIncFreq, sinWaveMag;
    
        /* 
            Based on numSinWave information, create the input data. The
            input data is first created using floating point dataType. The
            floating point data type is then converted to the appropriate
            fixed point notation
        */
        /* Clear the input floating point array */
        for (i = 0; i < N; i++) {
            x_ref_float[2*i] = (float)0.0;      
            x_ref_float[2*i + 1] = (float)0.0;  
        }
    
        /* Calculate the incremental freq for each sin wave */
        sinWaveIncFreq = ((float)3.142)/(numSinWaves*(float)1.0);
    
        /* Calculate the magnitude for each sin wave */
        sinWaveMag = (float)1.0/(numSinWaves * (float)1.0*N);
    
        /* Create the input array as sum of the various sin wave data */
        for (j = 0; j < numSinWaves; j++) {
            for (i = 0; i < N; i++) {
                x_ref_float[2*i] += sinWaveMag * (float)cos(sinWaveIncFreq*j*i);        
                x_ref_float[2*i + 1] = (float) 0.0;
            } 
        }
            
        /* Convert the floating point data to reference fixed point data */ 
        for (i = 0; i < N; i++) {
            x_ref[2*i] = x_ref_float[2*i] * 2147483648;     
            x_ref[2*i + 1] = x_ref_float[2*i + 1] * 2147483648;
        }
        
        /* Copy the reference input data to the various input arrays */     
        for (i = 0; i < N; i++) {
            x_16x16[2*i] = (x_ref[2*i] >> 16);      
            x_16x16[2*i + 1] = (x_ref[2*i + 1] >> 16);
    
            x_16x32[2*i] = x_ref[2*i] >> SCALE;     
            x_16x32[2*i + 1] = x_ref[2*i + 1] >> SCALE;
    
            x_32x32[2*i] = x_ref[2*i] >> SCALE;     
            x_32x32[2*i + 1] = x_ref[2*i + 1] >> SCALE;
        }
    }
    
    /* 
        The seperateRealImg function separates the real and imaginary data
        of the FFT output. This is needed so that the data can be plotted
        using the CCS graph feature
    */
    
    int16_t y_real_16x16  [N];
    int16_t y_imag_16x16  [N];
    
    int32_t y_real_16x32  [N];
    int32_t y_imag_16x32  [N];
    
    int32_t y_real_32x32  [N];
    int32_t y_imag_32x32  [N];
    
    seperateRealImg () {
        int32_t i, j;
    
        for (i = 0, j = 0; j < N; i+=2, j++) {
            y_real_16x16[j] = y_16x16[i];
            y_imag_16x16[j] = y_16x16[i + 1];
    
            y_real_16x32[j] = y_16x32[i];
            y_imag_16x32[j] = y_16x32[i + 1];
    
            y_real_32x32[j] = y_32x32[i];
            y_imag_32x32[j] = y_32x32[i + 1];
        }
    }
    
    /*
        The main function that implements the example functionality.
        This example demonstrates the usage of the various FFT kernels provided 
        with the C6x DSPLIB. The example shows:
            - Twiddle factor generation for the various kernels
            - Needed scaling to get correct output
            - Demonstrates usage of FFT APIs
    */
    
    void main () {
        /* Generate the input data */
        generateInput (NUM_SIN_WAVES);
        
        /* Genarate the various twiddle factors */
        gen_twiddle_fft16x16(w_16x16, N);
        gen_twiddle_fft16x32(w_16x32, N);
        gen_twiddle_fft32x32(w_32x32, N, 2147483647.5);
    
        /* Call the various FFT routines */
        DSP_fft16x16(w_16x16, N, x_16x16, y_16x16);
        DSP_fft16x32(w_16x32, N, x_16x32, y_16x32);
        DSP_fft32x32(w_32x32, N, x_32x32, y_32x32);
    
        /* Call the test code to separate the real and imaginary data */
        seperateRealImg ();
    }
    
    /* ======================================================================== */
    /*  End of file:  fft_example.c                                             */
    /* ------------------------------------------------------------------------ */
    /*            Copyright (c) 2011 Texas Instruments, Incorporated.           */
    /*                           All Rights Reserved.                           */
    /* ======================================================================== */
    
    

  • Hi Robert,

    The warning is introduced because the cmd file is missing or these sections are not declared by the cmd("../C6678.cmd"). You must specify a suitable cmd file for the project. The dsplib_c66x_x_x_x_x\examples\lnk.cmd could be used for FFT test. Copy it to your project root directory and rebuild the project.

    Allen

  • You got these errors when: Show Build Setting -> General :

    Advanced settings 

    Linker command file: the file either is not selected or wrong one