This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

HOW can dm365 encode with 2 fields (odd and even)

Hello,

We're working on DM 365 platform, the software setup is:

DVSDK: 2_10_01_18

XDCTOOLS: 3_15_01_59

MODE:option.mode = 1

I got interlaced UYVY data ,resized to YUV420SP ,encoded to H264 ,and  then sent to decoder, i can see a lot of mice teeth(combing) in the pictrue when moving,i want use the DEI  algorithm but i can't get it , so i want to encode the interlaced data with 2 fields, i don't know this is the right way , can you tell me more details ?

Regards

Yangchar