Hi Everyone
I'm having trouble configuring GPIO I/O lines on my Torpedo DM3730 chip for both input and output. I have been following a set of instructions from LogicPD [support.logicpd.com/downloads/1534/] concering the use of the 'sysfs' gpio library interface.
No software errors are encountered and I have checked that gpiolib is correctly configured during kernel compilation.....attempted on 4 seperate GPIO pins but can never seem to output the required 1.8V logic signal or read in any logic signals as input.
More info about what I have been attempting is on this WIKI: http://www.armadeus.com/wiki/index.php?title=GPIOlib
Any help would be fantastic
Thanks
Chris