Other Parts Discussed in Thread: DM3730
I'm optimizing the boot speed of our custom DM3730 board which use a uSB332x transceiver.
I found that in the kernel code drivers/usb/host/ehci-omap.c psp 04.02.00.07 after issuing ULPI command the condition tested for the command completion is
while ((ehci_omap_readl(omap->ehci_base, EHCI_INSNREG05_ULPI)
& (1 << EHCI_INSNREG05_ULPI_CONTROL_SHIFT))) {
cpu_relax();
if (time_after(jiffies, timeout)) {
dev_dbg(omap->dev, "phy reset operation timed out\n");
break;
}
}
This condition is never met and always times out.
Is the same of u-boot/drivers/usb/ulpi/ulpi-viewport.c
static int ulpi_wait(struct ulpi_viewport *ulpi_vp, u32 mask)
{
int timeout = CONFIG_USB_ULPI_TIMEOUT;
/* Wait for the bits in mask to become zero. */
while (--timeout) {
if ((readl(ulpi_vp->viewport_addr) & mask) == 0)
return 0;
udelay(1);
}
return ULPI_ERROR;
}
while in the u-boot/drivers/usb/ulpi/omap-ulpi-viewport.c
you changed in
static int ulpi_wait(struct ulpi_viewport *ulpi_vp, u32 mask)
{
int timeout = CONFIG_USB_ULPI_TIMEOUT;
while (--timeout) {
if ((readl(ulpi_vp->viewport_addr) & mask))
return 0;
udelay(1);
}
return ULPI_ERROR;
}
Is something specific for omap usb host controller or there is some problem in my hardware I should check?
Kind regards
Andrea