Other Parts Discussed in Thread: AM3517
Hi,
I have problems to boot WinEC7 on our self-made core module. We are using AM3517 CPU and the provided BSP from Adeneo.
After I start the image on the core module I get the following debug messages:
Windows CE Kernel for ARM (Thumb Enabled) Built on Jan 6 2011 at 16:15:31
ProcessorType=0c08 Revision=7 CpuId=0x411fc087
OEMAddressTable = 8041f8e0
INFO:OALLogSetZones: dpCurSettings.ulZoneMask: 0xb
CPU CP15 Control Register = 0xc5387d
CPU CP15 Auxiliary Control Register = 0x72
Initializing VFP, FPSID=410330c1
SysClock calibrate Frequency = 32768
OALInitRTC: RTC found on I2C bus. Turning it on now
NKStartup done, starting up kernel. nCpus = 1
Windows CE KernelInit
Error Reporting Memory Reserved, dump size = 0004b000
Booting Windows CE version 7.00 for (ARM)
Memory Configuring: Total pages: 35009, Filesystem pages = 17504
Booting kernel with clean memory configuration:
Total Memory Sections:2
[0] (static): start: 866f0000, extension/attributes: 0001f000, length: 078c1000
[1] (static): start: 8e000000, extension/attributes: 00004000, length: 01000000
Scheduling the first thread.
PID:00400002 TID:00410002 PGPOOL: Reserved 768 pages for Loader pool
PID:00400002 TID:00410002 PGPOOL: Reserved 256 pages for File pool
PID:00400002 TID:00410002 Message Queue support initialized, g_hMsgQHeap = c44a0010
PID:00400002 TID:00510002 FileSystem Starting - starting with clean file system
PID:00400002 TID:00510002 Initializing RTC
PID:00400002 TID:00510002 Initializing RTC
PID:00400002 TID:00510002 Value [Locale] without corresponding LCType in NLS Override section
PID:00400002 TID:00510002 Value [LocaleName] without corresponding LCType in NLS Override section
PID:00400002 TID:00510002 Warning! Kernel DLL 'k.locale.dll' is registered for thread creation/deletion notification. To improve performance if you dont need thread notifications call DisableThreadLibraryCalls from inside DPID:00400002 TID:00510002 Warning! Kernel DLL 'k.normalize.dll' is registered for thread creation/deletion notification. To improve performance if you dont need thread notifications call DisableThreadLibraryCalls from insidPID:00400002 TID:00510002 FSVOL: Using system database volume "\Windows\Registry\default.vol"
PID:00400002 TID:00510002 FSVOL: OEM forcing clean system db volume!
PID:00400002 TID:00510002 Warning! Kernel DLL 'bcrypt.dll' is registered for thread creation/deletion notification. To improve performance if you dont need thread notifications call DisableThreadLibraryCalls from inside DLLPID:00400002 TID:00510002 FSDMGR: DEBUGCHK failed in file d:\chelanrtm14\private\winceos\coreos\storage\fsdmgr\volumeapi.cpp at line 402
PID:00400002 TID:00510002 DEBUG_BREAK @ef822bf4 Ignored.
PID:00400002 TID:00510002 Unknown: DEBUGCHK failed in file d:\chelanrtm14\private\winceos\coreos\filesys\reg\profiles\secstor.h at line 487
PID:00400002 TID:00510002 DEBUG_BREAK @efd5e7c4 Ignored.
PID:00400002 TID:00510002 Value [Locale] without corresponding LCType in NLS Override section
PID:00400002 TID:00510002 Value [LocaleName] without corresponding LCType in NLS Override section
PID:00400002 TID:00510002 !!!WARNING: Mutually dependent DLL detected: FPCRT (pMod = 0xc040634c)
PID:00400002 TID:00510002 Warning! Kernel DLL 'k.ole32.dll' is registered for thread creation/deletion notification. To improve performance if you dont need thread notifications call DisableThreadLibraryCalls from inside DLPID:00400002 TID:00510002
Initializing Database
PID:00400002 TID:00510002 Warning! Kernel DLL 'k.sorting.dll' is registered for thread creation/deletion notification. To improve performance if you dont need thread notifications call DisableThreadLibraryCalls from inside PID:00400002 TID:00510002 SetCurrentUser: User hives not supported -- using same registry for all users
PID:00400002 TID:00510002 FSDMGR: DEBUGCHK failed in file d:\chelanrtm14\private\winceos\coreos\storage\fsdmgr\volumeapi.cpp at line 402
PID:00400002 TID:00510002 DEBUG_BREAK @ef822bf4 Ignored.
PID:00400002 TID:00510002 Unknown: DEBUGCHK failed in file d:\chelanrtm14\private\winceos\coreos\filesys\reg\profiles\secstor.h at line 487
PID:00400002 TID:00510002 DEBUG_BREAK @efd5e7c4 Ignored.
PID:00400002 TID:00510002 CePerf.dll is absent - performance data will not be recorded
PID:00400002 TID:0085001E Read: Attempts = 2
PID:00400002 TID:00C5001E
Faulted in KCall, PC = 8048345c, SP = ffff1014, args = 00000004 ffff1088 00000807!!
PID:00400002 TID:00C5001E Original Context when thread faulted:
PID:00400002 TID:00C5001E Exception 'Data Abort'(4) Thread-Id=00c5001e(pth=c040a720) PC=eff340d4 BVA=ffff1088, dwInfo = 00000807
PID:00400002 TID:00C5001E R0=ef9b4e3c R1=00000000 R2=00000000 R3=00000000
PID:00400002 TID:00C5001E R4=00004444 R5=00005555 R6=00006666 R7=00007777
PID:00400002 TID:00C5001E R8=00008888 R9=00009999 R10=00001010 R11=00001111
PID:00400002 TID:00C5001E R12=cc7afe8c SP=cc7afe74 Lr=eff14504 PC=eff340d4, Psr=0000001f
PID:00400002 TID:00C5001E Context when faulted in KCall:
PID:00400002 TID:00C5001E Exception 'Data Abort'(4) Thread-Id=00c5001e(pth=ffff0e48) PC=8048345c BVA=ffff1088, dwInfo = 00000807
PID:00400002 TID:00C5001E R0=ffff1088 R1=00000004 R2=60000193 R3=ffffc800
PID:00400002 TID:00C5001E R4=80427efc R5=00000000 R6=00000000 R7=eff340d4
PID:00400002 TID:00C5001E R8=00008888 R9=00009999 R10=00001010 R11=00001111
PID:00400002 TID:00C5001E R12=ffffb038 SP=ffff1014 Lr=8042b160 PC=8048345c, Psr=60000193
PID:00400002 TID:00C5001E Exception 'Data Abort' (0x4): Thread-Id=00c5001e(pth=c040a720), Proc-Id=00400002(pprc=866d2ad0) 'NK.EXE', VM-active=00400002(pprc=866d2ad0) 'NK.EXE'
PID:00400002 TID:00C5001E PC=8048345c(kernel.dll+0x0002d45c) RA=8042b160(NK.EXE+0x0001b160) SP=ffff1014, BVA=ffff1088
PID:00400002 TID:00C5001E RtlDispatchException: returning failure. Flags=0
PID:00400002 TID:00C5001E NK Kernel: DEBUGCHK failed in file d:\chelanrtm14\private\winceos\coreos\nk\kernel\apicall.c at line 1210
What could be the problem? Does anybody have an idea?
Best regards,
Andreas