This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Using a bit-banging GPIO I2C driver



Because the hardware on our board was soldered wrong way, I want to exchange the SDA and SCL pins of SPI bus 3 on the OMAP3.

What I'm trying now is to use a bit-banging GPIO driver and use it to drive the pins as GPIO.

In the board file I added the following:

static struct i2c_gpio_platform_data my_gpio_i2c_pdata = {
        .sda_pin        = 184,
        .scl_pin        = 185,
        .udelay         = 2,    /* 250 KHz */
        .timeout        = HZ,
};

static struct platform_device maple_gpio_i2c = {
        .name           = "i2c-gpio",
        .id             = 2,
        .dev            = {
                .platform_data  = &my_gpio_i2c_pdata,
        },
};


static int __init ....()
{

...
        /* Use bit-bang for I2C bus 3 because the wiring is wrong */
        printk(KERN_WARNING "Registering GPIO I2C driver now\n");
        if (platform_device_register(&maple_gpio_i2c) != 0)
                printk(KERN_WARNING "Failed to register i2c-gpio driver\n");

...


}

I see the "Registering GPIO I2C driver now" output on the kernel console when it boots, no failure message, but no I2C device is created. What did I miss?