Other Parts Discussed in Thread: OMAP-L138
Hi
Can not find any information about the type of input pin for ecap (TTL..,Schmitt trigger..)? What are the requirements (max rise time) for the ecap input signal?
Best regards
Thomas
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Other Parts Discussed in Thread: OMAP-L138
Hi
Can not find any information about the type of input pin for ecap (TTL..,Schmitt trigger..)? What are the requirements (max rise time) for the ecap input signal?
Best regards
Thomas
Hello,
See recommended operating conditions in data sheet. A generic I/O pin may use 1.8V or 3.3V LVTTL/LVCMOS, according to your hardware's DVDD.
OMAP-L138 (sprs586d.pdf), for example, requires max rise time of 10 ns or one fourth of the signal's period, whichever is less (see 4.2). Specific eCAP timing is given in 5.28.
Jakez