Other Parts Discussed in Thread: TMS320C6678
I have a question on the clock enable in the power on sequence of TMS320C6678. According to the data manual of 6678, “Once CVDD is valid, the clock drivers should be enabled. Although the clock inputs are not necessary at this time, they should either be driven with a valid clock or held in a static state with one leg high and one leg low.”
Now I cannot do that. My clock(DDRCLK, CORECLK,SRIOCLK for DSP will keep to be high impedance until 1.5V IO is on. Does this cause a problem for DSP booting? Please advise.
Best Regards,
John