This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DM8168 / SATA1 drive issue

The cutomser has the current issues with the DM8168 eval (EZ-DSK);
 
 - When booting with a SATA1 drive connected to the eval, the eval does not recognize the SATA1 drive. The following error is identified: 'SATA link down'. However if he disconnects/reconnects the SATA1 drive to the eval, the drive is recognized??
- -It looks like I can get a SATA2 disk to attach fairly reliably. Sata1 still has problems. I’m thinking this is a software issue, since hardware should work better with the lower frequency bus.

Comments...

-Tom-