Problem
Using an embedded Linux kernel (based on 2.6.32), we are able to successfully read data via DMA from McBSP2. However, with the same DMA configuration applied to McBSPs 3 and 4, DMA reads from those McBSPs fail to trigger the McBSP to actually read data from the DRR register of the respective McBSP, and the kernel eventually hangs. Even though the DMA transfer has been configured to trigger on a full frame of elements (DMA4_CCR register for logical DMA channel: FS = 1, BS = 0), it's as if the DMA transfer is instead triggering on a block or packet of frames.
Configuration (same for McBSPs 2, 3, 4)
Embedded Linux kernel version: 2.6.32.
Processor: AM3517
Custom mcbsp.c file (linux-2.6.32/arch/arm/plat-omap/mcbsp.c)
Total length of request buffer passed into kernel (omap_mcbsp_recv_buffer) from userspace: 3584 bytes (896 4-byte elements)
DMA element size: 4 bytes (32 bits)
Number of elements per frame: 14 (programmed into DMA4_CEN register)
Number of frames : 896 / 14 = 64 (programmed into DMA4_CFN register).
I've confirmed that the correct HW DMA request lines are selected for the respective McBSPs and programmed into the DMA4_CCR register bits 20:19,4:0.
I've also confirmed the correct pad configuration register settings for McBSPs 2-4.
Using a scope, I've confirmed that CLKX and FSX show clock and frame sync pulses on their correct pins.
With this configuration, DMA transfers from McBSP2 DRR into a local buffer occur with no issues.
Attempted DMA transfers from McBSP3 DRR or McBSP4 DRR into a local buffer hang the kernel.
McBSP 2 registers prior to omap_start_dma method:
DXR: 0x00000000
SPCR2: 0x000000c7
SPCR1: 0x00000003
RCR2: 0x00000000
RCR1: 0x00000ea0
XCR2: 0x00000001
XCR1: 0x00000ea0
SRGR2: 0x000021df
SRGR1: 0x00000004
MCR2: 0x00000201
MCR1: 0x00000201
RCERA: 0x00007ffe
RCERB: 0x00000000
XCERA: 0x00007fff
XCERB: 0x00000000
PCR0: 0x00000f00
RCERC: 0x00000000
RCERD: 0x00000000
XCERC: 0x00000000
XCERD: 0x00000000
RCERE: 0x00000000
RCERF: 0x00000000
XCERE: 0x00000000
XCERF: 0x00000000
RCERG: 0x00000000
RCERH: 0x00000000
XCERG: 0x00000000
XCERH: 0x00000000
REV: 0x00000023
RINTCLR: 0x00000000
XINTCLR: 0x00000000
ROVFLCLR: 0x00000000
SYSCON: 0x00000214
THRSH2: 0x0000000e
THRSH1: 0x0000000d
IRQST: 0x0000471e
IRQEN: 0x00000000
WAKEUPEN: 0x00000408
XCCR: 0x00000008
RCCR: 0x00000008
XBUFFSTAT: 0x00000500
RBUFFSTAT: 0x0000037f
SSELCR: 0x00000084
STATUS: 0x00000000
CLKX_FSX: 0x01000100
DX_DR: 0x00000100
*** MCBSP padconf registers ***
mcbsp2_reg1 (reg addr 0x4800213C) 0x01000100
mcbsp2_reg2 (reg addr 0x48002140) 0x00000100
mcbsp3_reg1 (reg addr 0x4800216C) 0x01000000
mcbsp3_reg2 (reg addr 0x48002170) 0x01000100
mcbsp4_reg1 (reg addr 0x48002184) 0x01000100
mcbsp4_reg2 (reg addr 0x48002188) 0x01000000
*** CM_FCLKEN_PER register: 0x0000080f ***
*** CM_ICLKEN_PER register: 0x0003e80f ***
*** CONTROL_DEVCONF0 register: 0x04000000 ***
*** CONTROL_DEVCONF1 register: 0x00000000 ***
*** DMA_CCR register: 0x01084022 ***
*** CIRC register for dma logical channel: 0x00000922 ***
McBSP 4 registers prior to omap_start_dma method
DXR: 0x00000000
SPCR2: 0x000000c7
SPCR1: 0x00000003
RCR2: 0x00000000
RCR1: 0x00000ea0
XCR2: 0x00000001
XCR1: 0x00000ea0
SRGR2: 0x000021df
SRGR1: 0x00000004
MCR2: 0x00000201
MCR1: 0x00000201
RCERA: 0x00007ffe
RCERB: 0x00000000
XCERA: 0x00007fff
XCERB: 0x00000000
PCR0: 0x00000f00
RCERC: 0x00000000
RCERD: 0x00000000
XCERC: 0x00000000
XCERD: 0x00000000
RCERE: 0x00000000
RCERF: 0x00000000
XCERE: 0x00000000
XCERF: 0x00000000
RCERG: 0x00000000
RCERH: 0x00000000
XCERG: 0x00000000
XCERH: 0x00000000
REV: 0x00000013
RINTCLR: 0x00000000
XINTCLR: 0x00000000
ROVFLCLR: 0x00000000
SYSCON: 0x00000214
THRSH2: 0x0000000e
THRSH1: 0x0000000d
IRQST: 0x0000473e
IRQEN: 0x00000000
WAKEUPEN: 0x00000408
XCCR: 0x00000008
RCCR: 0x00000008
XBUFFSTAT: 0x00000080
RBUFFSTAT: 0x0000007f
SSELCR: 0x00000084
STATUS: 0x00000000
CLKX_FSX: 0x01000100
DX_DR: 0x00000100
*** MCBSP padconf registers ***
mcbsp2_reg1 (reg addr 0x4800213C) 0x01000100
mcbsp2_reg2 (reg addr 0x48002140) 0x00000100
mcbsp3_reg1 (reg addr 0x4800216C) 0x01000000
mcbsp3_reg2 (reg addr 0x48002170) 0x01000100
mcbsp4_reg1 (reg addr 0x48002184) 0x01000100
mcbsp4_reg2 (reg addr 0x48002188) 0x01000000
*** CM_FCLKEN_PER register: 0x0000080f ***
*** CM_ICLKEN_PER register: 0x0003e80f ***
*** CONTROL_DEVCONF0 register: 0x04000000 ***
*** CONTROL_DEVCONF1 register: 0x00000000 ***
*** DMA_CCR register: 0x01004034 ***
*** CIRC register for dma logical channel: 0x00000922 ***
Major differences between McBSP 2 and 4
Comparing IRQST between both McBSPs show that McBSP 4 is in overflow, indicating that the McBSP hasn't been triggered to read data from DRR.
Comparing RBUFFSTAT between both McBSPs: number of occupied locations in McBSP 2 RB is 895 (0x37F); number of occupied locations in McBSP 4 RB is 127 (0x07F); maybe this difference is due to RBUFFSTAT field width differences between the two McBSPs.
Workaround to prove basic McBSP functionality
Finally decided to decrease the number of frames in the DMA transfer on McBSP 4 from 64 to 9.
Using configuration from above (except for number of frames), this equates to a DMA transfer of 14 * 9 = 126 4-byte elements.
DMA transfers are successful using this configuration, however this change will not work with our current application design.
Questions
- Am I configuring something incorrectly in the DMA transfer for syncing on a frame? If so, is there a correct way to configure the DMA?
- Is there a known problem in the 2.6.32 kernel related to DMA transfers not working on McBSP3 and 4 of the AM3517 processor?
Any tips or suggestions are greatly appreciated.
Thanks for your time,
Tony