This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Which media formats are supported by HW-accelerated video decoder in 4AI.1.5 ICS release?



Dear All

Which media formats are supported by HW-accelerated video decoder in 4AI.1.5 ICS release?

Paul

  • Hi Pavel,

    The following video & audio decoders are supported by HW-accelerated video decoder in 4AI.1.x ICS releases.

    Video Decoders

    ----------------------

    MPEG1 Dec
    1080p30 (5/6)
    20Mbps
    MPEG2 MP@ML Dec
    1080p30 / 1080i60
    20Mbps
    MPEG2 MP@HL Dec
    1080p30 / 1080i60
    20Mbps
    H.263 P3L70
    1080p30
    20Mbps
    MPEG4 SP/ASP
    1080p30 /1080i60
    50Mbps
    VC-1 SP/MP/AP (WMV9) Dec
    1080p30 / 1080i60
    20Mbps
    H264 BP/MP Dec
    1080p30 / 1080i60
    50Mbps (CAVLC)
    20Mbps (CABAC)
    H264 HP Dec
    1080p30 / 1080i60
    25Mbps (CABAC)
    50Mbps (CAVLC)
    VP8
    1080p30
    <10Mbps
    H264 SEI s3D
    stereo 720p30
    20Mbps

    Audio Codecs (Dec)

    ----------------------------
    MP3
    WMA9
    WMA10 Pro
    WMA Lossless
    AAC-LC
    HE-AAC-v1/AAC+
    HE-AAC-v2/eAAC+

    AMR-NB

    AMR-WB

    The following container parser formats are supported by 4AI.1.x releases.

    Container/Parser
    MIME type/
    Extension
    MPEG4
    mp4/m4a
    3GPP
    3gp
    3GPP2
    3gpp2
    MP3
    Mpeg
    AAC
    aac
    AMR
    Amr
    WAV
    wav 
    JPEG
    jpg 

    Thanks & Best Regards,

    Venkat