Dear Sir/Madam,
I am using OMAP L138 processor which has DSP+ARM on it.
I want to use EMIF and uPP interface of OMAP. My requirement is mentioned below
- I have 252 ADC Channels, with each channel having 32 bits and this 252 channels will run with a loop kHz of 2 ie my datarate of ADC channel is 252*32*2000 = 16128000(16Mbps)
- Image sensor with resolution of 752 x 480 with each pixel of 10bits(consider 2bytes) and 60fps, for this datarate will be 752*480*16*60 = 346521600 (346Mbps)(consider full resolution), but we are not using full resolution and we are using maximum 400 x 200, for this datarate will be 400*200*16*60 = 76800000 (76Mbps).
Please suggest which interface (uPP/EMIF) will be better for two application and for which processor either ARM or DSP and also I want these two applications has to be run in parallel.
Waiting for your earlier response.
With Regards,
Prashant
9900142937