This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

OMAPL138 Boot Process and AISGEN tool Usage

Other Parts Discussed in Thread: OMAPL138

Hi,

I'm new to OMAP Processor Usage. Can any one give me clarity on the following questions

For OMAPL138 Booting Process i see multiple points in ti manuals and wiki - could not get the clear idea on how the process goes.

On Reset in OMAPL138, which boot ROM Code will execute ? DSP or ARM ?

Will DSP ROM Code, initiates the ARM Boot Loader ( U-boot ) ? Once ARM Booting is done, does it wakes up DSP in bootloader itself ?

What does AISGEN tool do ? I see it combines UBL and U-Boot and creates AISGEN Uboot Image. If i download this image on Flash of the board, on reset which ROM code calls this - is it DSP ROM or ARM ROM ?

Do we have a default code residing in OMAP ? Can AISGEN tool program  the ROM of ARM/DSP ?

Regards,

Chakra