This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

trouble in DSP code optimization



I have the following code:

       for(cc3=0; cc3<9; cc3++)
       {
            rfAddr = (Uint32)rfPreviousEnergy;
 
            while (1)  
           {
               if ((*((Uint32 *)rfPreviousEnergyCount)) == 0xFF)    break;
            }
        
            for (cc2 = 0; cc2<40; cc2++)
           {
                 // other codes
           }
        
           *((Uint32 *)rfPreviousEnergyCount) = cc3+1;
        
       }        

When I compile and build my project,  the codes runs as exepected if I do not use optimization, i.e. --opt_level=0 or 1.  However,  when I use --opt_level=2 or 3, this piece of  codes do not run  normally.  Specifically,  it halts at the "rfAddr = (Uint32)rfPreviousEnergy", and do not go to the next line "while loop".   When I checked the optimized disassembly codes, I found that the "while loop" dose not follow " rfAddr = (Uint32)rfPreviousEnergy".   Thus I wonder how I can make the execution of the code jumps to while loop?  Thanks!