This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AM335x PinMuxUtility

Guru 15520 points

Hi,

I have question about PinMuxUtility.
I'm using AM335x PinMuxUtility v2_04_01_00 and have confused with selecting GPMC Address pin.

There are pins named MUX0 or MUX1. What does this means?
My understanding was that it is necessary to select  same MUX# pin.
Otherwise "IO Set Violation" will occur. Is it wrong?

So I can't understand why "IO Set Violation" doesn't occur
when selecting  the following pins:
GPMC A0 MUX1 (ball:R1)
GPMC A1 MUX1 (ball:R2)
GPMC A2 MUX1 (ball:R3)
GPMC A3 MUX1 (ball:R4)
GPMC A4 MUX1 (ball:T1)
GPMC A5 MUX1 (ball:T2)
GPMC A6 MUX1 (ball:T3)
GPMC A7 MUX1 (ball:T4)
GPMC A12 MUX0 (ball:U1)
GPMC A13 MUX0 (ball:U2)
GPMC A14 MUX0 (ball:U3)
GPMC A15 MUX0 (ball:U4)
GPMC A8 MUX1 (ball:U5)
GPMC A9 MUX1 (ball:R5)
GPMC A10 MUX1 (ball:V5)
GPMC A11 MUX1 (ball:R6)

Best regards,
g.f.