This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Automation of NAND programming using FLASH v1.6.0.0 utility

Hello All,

We are using FLASH v1.6.0.0 utility for programming the NAND (for flashing the WinCE image onto NAND). We are flashing it using through USB.

Is there any options to make run these FLASH v1.6.0.0 utility commands using DOS prompt?

In production, we would like to automate the flashing of NAND by running a batch file etc. I am wondering whether we can automatically program all the images of WinCE by running a batch file which intern runs the instructions of FLASH v1.6.0.0 utility.

Thank you in advance for the reply.

Regards,

Mahesh Hooli