Hi Folks,
We are going to implement two ethernet ports (RMII) with AM335X. Our intention is to use only one 50MHz oscillator as source to four points: the REF_CLK of the two MACs on AM335X and the CLKIN input of each phy. So we are assuming to use a clock distributor / clock fanout buffer as a way to have a good signal at each point.
Question is: Clock distributors have a skew between each output line. In this particular scenario, what would be an acceptable skew value between the clock that source the MAC and the clock that source its respective PHY?
Take as reference a clock distributor from TI, the CDCLVC1106 that have a maximum skew of 50 ps (output to output).
Thanks,
Rodrigo