Hello,
I am facing an issue while executing the /usr/share/ti/j5eco-tvp5158/decoder_init during booting linux on the TI-JECO board with ezdk release version 5_05_00_04. Below are the logs,
I2C (0x58): Read ERROR !!! (reg[0x08], count = 5)
Error getting ChipId information Decoder_Init: VIP 0: VID DEC 0400 (0x58): 0000:0000:0000
Decoder_Init: Detect video in progress for inst 0 !!!
I2C (0x58): Write ERROR !!! (reg[0xfe], count = 1)
Error setting video mode I2C (0x58): Write ERROR !!! (reg[0xff], count = 1)
Error getting video status I2C (0x58): Write ERROR !!! (reg[0xff], count = 1)
Error getting video status I2C (0x58): Write ERROR !!! (reg[0xff], count = 1)
Error getting video status I2C (0x58): Write ERROR !!! (reg[0xff], count = 1)
Error getting video status Decoder_Init: Detect video Done: NO Video signal available in channel 0 !!!
I2C (0x58): Write ERROR !!! (reg[0xfe], count = 1)
Loading HDVPSS Firmware
SysLink version : 2.10.05.26
Could this be an hardware issue and What actually the decoder_init does ?
Thanks & Regards,
Rakesh