This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

SCD/Tamper Detection



Hi guys,
I have some troubles with SCD/tamper Detection in the latest RDK

If I use
RDK 02.00.00.24, it seems to work (I see line [TAMPER DETECTED]... in the console), while if I use RDK 02.80.00.10, it seems not.
Motion Detection works with both RDKs

The setup is the same in both cases: demo 1, used prebuilt images, same video signals.

Any helps?

Best Regards

Ivan

  • By following steps, I can see the motion.

    A:
     =========
     Main Menu
     =========
     1: VCAP + VENC + VDEC + VDIS  - Progressive SD Encode + Decode

    B:
     =============
     Run-Time Menu
     =============
     1: Capture Settings

    C:
     =====================
     Capture Settings Menu
     =====================
     ...
     e: Live Motion Detection (LMD) Configuration

    D:
     ...
     Enter LMD block enable/disable flag [Valid values, 0 .. 1] :1
     ...