This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Function of Ethernet cable in EVM

Hi,

What exactly the ethernet connection is used for in the 6678 EVM?

I mean when we're not using NDK, UDP, ethernet boot mode...

Can I use only the USB JTAG? Or there's a communication between PC and the EVM that is done using the ethernet cable and if I disconnect it, I won't be able to load programs, debug, etc..?

Thanks

  • Johannes,

    The Ethernet cable is not required if you are "not using NDK, UDP, ethernet boot mode."

    For my case, I do not know much about the NDK other than it has all the APIs you need to make communication across the Ethernet port easy. I do not have any test cases I run that use it.

    So, I almost never have an Ethernet cable connected to my EVM6678. In fact, most of the time the only connections I have to the board are power and my USB cable for emulation.

    Regards,
    RandyP