Hi,
I am new to OMAP4 processors. I got hold of Public TRM for OMAP4's 4460 processor. I am doing power measurements as part of my project on Samsung Galaxy Nexus. I have some questions regarding this -
1] Does both the CPU's on 4460 processor are power gated separately? If yes, can you refer to the section in TRM that explains this? I didn't find any.
2] Is my understanding correct, that 4460 CPU's are single clock'ed? and to put the CPU in Retention mode, the clock is gated where as to put in OFF mode the CPU's are power gated?
3] The latency values to put the CPU is one of the C-states are hard-coded in the Linux_v3.0.8. For example, as per the time file in sysfs in /sys/devices/system/....cpuo/time for state3 it is defined as 1500us whcih is defined as the time taken from idle task to wfi and from wfi to task context. How are these values measured?
Thanks for your time and appreciate your response.
Best Regards
Siva Penke