This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Display Driver for OMAP



I need 33 MHz pixel clock and I set the dividor to 3 (I think my clock is 96MHz) and logic clock dividor to 1. I saw the text displayed on the LCD, but it was blurring and the screen is not stablized. My screen size is not standard (800 * 480).

 

Anything I should try - the same display driver works for a 24 MHz NEC display (640 * 480) the divisor was 4 and logic clock divisory was 1.

 

Thanks.

 

Annie