This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

the problem when use uart1 on dm368

Hi all!

Now we want to use the uart1 on dm368.

but we can only send data and can't receive response.

the serial's info as follow:

# cat /proc/tty/driver/serial
serinfo:1.0 driver revision:
0: uart:16550A mmio:0x01C20000 irq:40 membase 0xFBC20000 tx:413 rx:20 RTS|CTS|DTR|DSR
1: uart:16550A mmio:0x01D06000 irq:41 membase 0xFBD06000 tx:0 rx:0 CTS|DSR

# cat /proc/interrupts
           CPU0
  0:          0       AINTC  csl
  1:          0       AINTC  csl
  2:          0       AINTC  csl
  3:          0       AINTC  csl
  4:          0       AINTC  csl
  5:          0       AINTC  csl
  6:          0       AINTC  csl
  8:       8709       AINTC  davinci_osd
 16:          0       AINTC  EDMA Completion
 17:          0       AINTC  EDMA CC Error
 18:          0       AINTC  EDMA TC0 Error
 19:          0       AINTC  EDMA TC1 Error
 26:        295       AINTC  davinci-mmc
 29:          4       AINTC  rtc0
 32:      14554       AINTC  clockevent
 33:          0       AINTC  free-run counter
 39:          0       AINTC  i2c_davinci
 40:        124       AINTC  serial
 52:          0       AINTC  mac_rx_threshold
 53:       2620       AINTC  mac_rx
 54:          0       AINTC  mac_tx
 55:          0       AINTC  mac_misc
 61:          0       AINTC  EDMA TC2 Error
 62:          0       AINTC  EDMA TC3 Error

we can't find uart1's irq in the table

Is it the reason why uart1 can't receive data?

what should we do for this?

Best regards!