Other Parts Discussed in Thread: TMS320C5515
Hi,
I have a TMS320C5515 EVM that I am running tests on using the CSL. In the directions it says:
TEST PROCEDURE:
- Insert "SD" card into the MMC/SD socket(J9) on the C5505/C5515 EVM
- Open the CCS and connect the target (C5505/C5515 EVM)
- Open the project "CSL_MMCSD_MmcCardExample_Out.pjt" and build it
- Load the program on to the target
- Set the PLL frequency to 12.288MHz
- Run the program and observe the test result
- Repeat the test at PLL frequencies 40, 60, 75 and 100MHz
- Repeat the test in Release mode
Where do I set the PLL frequency in Code Composer? I am ashamed to say this, but I have performed this once on accident and cannot find it in the menus any longer.
Thank you for your help in advance.
Dozier