Other Parts Discussed in Thread: TWL6040
Dear Sir,
I would like to use Blaze board to verify the audio path functionality from HS mic to headphone/headset output(UL to DL1), below is the link what I refer to,
http://omappedia.org/wiki/File:ASoC_ABE_controls.jpg
http://omappedia.org/wiki/File:ASoC_ABE_volumes.jpg
and the commands I used as below,
tinymix 50 1
tinymix 51 1
tinymix 9 126
tinymix 72 "HS DAC"
tinymix 73 "HS DAC"
tinymix 67 13
tinymix 36 1
tinymix 23 120
tinymix 63 "None"
tinymix 62 "None"
tinymix 55 "AMic0"
tinymix 54 "AMic1"
tinymix 20 130
tinymix 77 "Headset Mic"
tinymix 76 "Headset Mic"
tinymix 64 1
tinymix 65 4
tinymix 24 0
tinymix 25 0
tinymix 26 0
tinymix 33 0
tinymix 71 0
tinymix 34 1
tinyplay test1.wav &
tinycap test.wav -d 1 -c 2 -r 48000 -b 16 -C
the result would be casued a noisy sound around the Blaze board, and it seems the HS mic can not do the capturing function normally.
Could you correct me if some paths I set up incorrectly?
thx~