I want to update my Linux Platform Support Packages from psp03.01.01.39(linux-2.6.32) to psp03.21.00.04(linux-2.6.36) so it can support more functionality as i wished.
But i meet build problem in DMAI package because some enum values are not supported in linux-2.6.36 kernel header file.
Is there a correct DMAI package which is verified on linux-2.6.36 ?
Regards, James