Hi All,
We are currently designing a system using an AM3352 with the TPS65910 PMIC. We do not require the RTC-only low power mode of the AM3352 and are not planning to include an RTC crystal.
SPRS717 Figure 4-5 indicates that the PMIC_POWER_EN output is not available when the RTC feature is disabled. From what I have seen, all the reference designs appear to use the PMIC_POWER_EN signal to trigger the PMIC to power on the MPU. If the PMIC_POWER_EN output is not available, is there a recommended way to signal to the PMIC to power on the AM3352 or can the PWRHOLD signal of the PMIC simply be pulled-up permanently?
Kind Regards
Mark