This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

OMAP L138 NAND boot issue with Hynix HY27US08121B (64 MB 1bit ECC)

Other Parts Discussed in Thread: OMAPL138

Hi,

We are using hynix HY27US08121B, 64 MB,1 bit ECC nand in our custom board. I'm using Lauterbach / PEEDI debugger to program the NAND flash, as the CCS nand write program does not support for our memory device ( As per the readme file in nand write, it support only for nand device with 4 bit ECC, Let me know If any one has suggestion to change it for 1 bit ECC)

I could write to nand with Lauterbach debugger, but flash verify failed. When i dump the flash and see all data are 0xFF.

 For testing we made the CE hardware line pulled low permanently, then flash program and verify successful, but NAND boot is not successful. I have verified the BOOT mode is set to NAND with debugger.

To check RBL, I erased the nand and reset/run/stop, then when i check the NANDFCR register the 4-bit ECC is enabled by RBL. Our RBL version is d800k008.

I would like to know the RBL supports for our nand flash with 1 bit ECC ?.  Any suggestion why the nand verify fails without pulling the CE line low. We have probed the hardware lines, all seems to be ok as per the omap reference manual.

Thanks & Regards,

Arul.