Other Parts Discussed in Thread: SYSBIOS, TPIC2810
I have the IDK SYSBIOS examples, which compile and the GEL file initializes a Sitara 3359 15x15 target. The compiler is Version: 5.2.0.00069.
I tried the boot and demo projects, but they have hardware that is not on the ICE (CPLD on I2C, LCD etc). Is there source code for the demo that ships with the ICE kit (or source besides the Beckhoff IP)? At the moment I just want to get the low-level stuff up, and even programming the row of LEDs on the I2C connected TPIC2810 or the multi-coloured LEDs would be great.
Even a few files would be helpful and I am happy to debug via JTAG.
Thanks,
Ian Clark