This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Shared library problem in android



My .so File Info:

"libvcsFPClient.so: ELF 32-bit LSB shared object, ARM, version 1 (SYSV), dynamically linked, not stripped."

So it was build in above environment.
Now problem is , while running the project it gives the following error log:
07-18 23:55:54.261: D/dalvikvm(638): Trying to load lib /data/data/com.example.hellojni/lib/libhello-jni.so 0x40ffa280 
07-18 23:55:54.271: D/dalvikvm(638): Added shared lib /data/data/com.example.hellojni/lib/libhello-jni.so 0x40ffa280 
07-18 23:55:54.271: D/dalvikvm(638): Trying to load lib /data/data/com.example.hellojni/lib/libvcsFPClient.so 0x40ffa280
 07-18 23:55:54.291: W/dalvikvm(638): Exception Ljava/lang/UnsatisfiedLinkError; thrown while initializing Lcom/example/hellojni/HelloJni; 
07-18 23:55:54.291: W/dalvikvm(638): Class init failed in newInstance call (Lcom/example/hellojni/HelloJni;)
 07-18 23:55:54.291: D/AndroidRuntime(638): Shutting down VM 
07-18 23:55:54.291: W/dalvikvm(638): threadid=1: thread exiting with uncaught exception (group=0x40a13300) 
07-18 23:55:54.322: E/AndroidRuntime(638): FATAL EXCEPTION: main 
07-18 23:55:54.322: E/AndroidRuntime(638): java.lang.ExceptionInInitializerError 
07-18 23:55:54.322: E/AndroidRuntime(638): at java.lang.Class.newInstanceImpl(Native Method) 
07-18 23:55:54.322: E/AndroidRuntime(638): at java.lang.Class.newInstance(Class.java:1319)
 07-18 23:55:54.322: E/AndroidRuntime(638): at android.app.Instrumentation.newActivity(Instrumentation.java:1053) 
07-18 23:55:54.322: E/AndroidRuntime(638): at android.app.ActivityThread.performLaunchActivity(ActivityThread.java:1974) 
07-18 23:55:54.322: E/AndroidRuntime(638): at android.app.ActivityThread.handleLaunchActivity(ActivityThread.java:2084)
 07-18 23:55:54.322: E/AndroidRuntime(638): at android.app.ActivityThread.access$600(ActivityThread.java:130) 
07-18 23:55:54.322: E/AndroidRuntime(638): at android.app.ActivityThread$H.handleMessage(ActivityThread.java:1195
) 07-18 23:55:54.322: E/AndroidRuntime(638): at android.os.Handler.dispatchMessage(Handler.java:99) 
07-18 23:55:54.322: E/AndroidRuntime(638): at android.os.Looper.loop(Looper.java:137) 
07-18 23:55:54.322: E/AndroidRuntime(638): at android.app.ActivityThread.main(ActivityThread.java:4745)
 07-18 23:55:54.322: E/AndroidRuntime(638): at java.lang.reflect.Method.invokeNative(Native Method) 
07-18 23:55:54.322: E/AndroidRuntime(638): at java.lang.reflect.Method.invoke(Method.java:511) 
07-18 23:55:54.322: E/AndroidRuntime(638): at com.android.internal.os.ZygoteInit$MethodAndArgsCaller.run(ZygoteInit.java:786) 
07-18 23:55:54.322: E/AndroidRuntime(638): at com.android.internal.os.ZygoteInit.main(ZygoteInit.java:553)
 07-18 23:55:54.322: E/AndroidRuntime(638): at dalvik.system.NativeStart.main(Native Method)
 07-18 23:55:54.322: E/AndroidRuntime(638): Caused by: java.lang.UnsatisfiedLinkError: Cannot load library: link_image[1891]: 36 could not load needed library 'libusb.so' for 'libvcsFPClient.so' (load_library[1093]: Library 'libusb.so' not found) 
07-18 23:55:54.322: E/AndroidRuntime(638): at java.lang.Runtime.loadLibrary(Runtime.java:370) 
07-18 23:55:54.322: E/AndroidRuntime(638): at java.lang.System.loadLibrary(System.java:535) 
07-18 23:55:54.322: E/AndroidRuntime(638): at com.example.hellojni.HelloJni.<clinit>(HelloJni.java:69)
 07-18 23:55:54.322: E/AndroidRuntime(638): ... 15 more 07-18 23:58:36.001: I/Process(638): Sending signal. PID: 638 SIG: 9
My Android.mk file:

LOCAL_PATH := $(call my-dir)

include $(CLEAR_VARS)

LOCAL_MODULE    := hello-jni
LOCAL_SRC_FILES := hello-jni.c

include $(BUILD_SHARED_LIBRARY)

include $(CLEAR_VARS)
LOCAL_MODULE                        := vcsFPClient
LOCAL_SRC_FILES                     := libvcsFPClient.so
include $(PREBUILT_SHARED_LIBRARY)



include $(CLEAR_VARS)
LOCAL_MODULE                        := usb
LOCAL_SRC_FILES                     := libusb.so
include $(PREBUILT_SHARED_LIBRARY)
How to link prebuilt cross compiler toolchain?
How to modify further .mk file ?
My system Properties are ,

Using ubuntu 10.04 , i686 .
GCC - 4.4.3