The TMDXEVM6678L board uses a 12V power input with a max of up to 18V, is it possible to power the board using a 15V nominal power supply?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
The TMDXEVM6678L board uses a 12V power input with a max of up to 18V, is it possible to power the board using a 15V nominal power supply?
The TMDEXEVM6678 was designed to operate with the provided 12V power supply. Although the power supply components on the board can be used with higher input voltages that would require changes to the passive components and the programming of the digital power supply controller.