USB0(OTG) port of AM3517 cannot connect specific USB memory.
When the USB memory cannot be connected, it seems to start a handshake again that the USB memory outputs first Chirp K two times during Chirp handshake.
In most cases, it may be said that the USB memory has some problem.
However I have concern for USB0(OTG) port of AM3517.
It is too early that the USB0(OTG) port starts Chirp KJKJKJ after first Chirp K.
Time between Chirp K and Chirp KJKJKJ is 2.22usec.
In the case of AM3517 HSUSB port , it is 92.99usec.
In the case of PC USB port, it is 3.2usec.
Is it bad to be 2.22usec?
If it is bad, is there the method to extend it?
Best regards,
Daisuke