This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

OMAP4 Ethernet Driver Issue

Hi,

            We wanted to try ethernet over usb on  on Blaze Tablet ( OMAP4460 processor running ICS android version) . I have a ASIX USB ethernet dongle and want it to be interfaced. Is there any steps available which i can use to bring up the ethernet interface.

The primary reason for going to USB ethernet is because the existing ethernet driver supports only upto 2Mbps throughput which is limiting our application. Any help on this is highly appreciated.

 

Thanks nad Regards,

Shantanu Bhaduri 

 

 

 

 

  • Shantanu,

    There is an application note that describes in detail how to use a USB-Ethernet adapter with the Blaze Tablet and how to obtain throughput measurements.  You can contact your TI representative for access to this document.  To summarize the key steps:

    1. Apply these patches to your kernel.  I believe that all but the last patch are already included if you are using the 4AI.1.6 release.  (These are needed to improve throughput performance, but are not required for basic USB-Ethernet functionality.)

    http://review.omapzoom.org/21630

    http://review.omapzoom.org/22482

    http://review.omapzoom.org/22486

    http://review.omapzoom.org/22487

    http://review.omapzoom.org/22488

    http://review.omapzoom.org/22489

    http://review.omapzoom.org/22490  

    2. Enable CONFIG_USB_USBNET in your menuconfig.  (This option is located in:  Device drivers --> Network device support --> USB network adaptors -> Multi-purpose USB networking framework.)

    3. Connect a self-powered USB hub to the USB OTG or EHCI port on the Blaze Tablet via the micro-A or standard-A USB cable, respectively.  You should see detection messages on the serial terminal.

    4. Connect the USB-Ethernet adapter to the self-powered USB hub.  You should see detection messages on the serial terminal.

    Let me know if you have any further questions.

    Regards,
    Gina 

  • Gina,

                  I have tried your suggestion and it works fine.

    Thanks a lot for your response

    Regards,

    Shantanu Bhaduri