This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Problems about PA_emacExample_exampleProject



       There are two C6678 DSPs on my board .  I am trying to implement C6678_A  sending data to C6678_B through ethernet interface.

I consulted an example project located at pdk_C6678_1_0_0_21\packages\ti \ drv \ exampleprojects\ PA_emacExample_exampleProject.

Here are my questions.

      1. In the example project, when the function Sendpacket() is executed, interrupt service handler(ISR)named Cpsw_RxISR() is called automatically.

How is this achieved?

I reffered to the .cfg file but found nothing.

      2. In my case,When the C6678_A finishes executing the function SendPacket() , it should send an interrupt to C6678_B.  Then C6678_B start call the

Cpsw_RxISR() automatilly.  To achieve this, how to modify the codes?

      3. Is there any document helping user to familiar with .cfg file?Every time I look up the .cfg file , i can get little information.

      Supplement : C6678_A and C6678_B runs different projects. C6678_A  does initialization and send data only . C6678_B does initialization and receive

data only. Both the projects are based on PA_emacExample_exampleProject.

                             Both SendPacket()  and Cpsw_RxISR() are located at cppi_qmss_mgmt.c.

        I hope someone coule help me . Thank you in advance.