This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

evmAM1808 & StarterWare - I need that match made in heaven

Other Parts Discussed in Thread: AM1808

I would like to purchase the development board that TI used to create the examples in the StarterWare package.  I have downloaded the AM1808 StarterWare package and the folder for all the examples shows an evmAM1808 for the platform of the AM1808 device.  Who makes this board and where can I buy it?  I just want the examples to work out-of-the-box so I can start my development on top of them.  I have the MityArm board right now and I am just having issues with it running the examples and would like to have the board that the examples were modeled after.

Thanks,

Tim

  • OK, I have received the board.  I have built the StarterWare AM1808 1_00_03_03 examples.  I have the traveler emulator.  When I try to debug with CCS 5, I am not sure what to do.  I have 2 SD cards that were included (Linux and Windows CE).  The DVD in the kit did not include a gel file, but I find some in the starterware folder.  What gel file should I use for the TMDXEVMWIFI1808L?  How do I turn on the unit to get it ready to receive the debugging from the emulator - do I just turn it on?  When I just turn it on without an SD card, I just get an error that says "Device OPP SD/MMC Boot failed.  Is that OK?

    Thanks.